AXIS#.IL.IVFB
Description
AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.IVFB is an offset value that is added to the measured current in the u-winding of the AXIS#.MOTOR. This value is used for compensating for an error in the current measurement. The drive measures 256 times the current in the u-winding when powering-up the drive. Afterwards, the drive calculates the average value of the measured current and uses this value for the offset value.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
A |
|
Range |
± Drive peak current (IPEAK) |
|
Default Value |
0 A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics